Post Go back to editing

Questions regarding AD8351: Is there a spice model?

I'm looking for a spice model fore the AD8351. I've loooked but it doesn't seem to be posted. Does any one have one?

jim

Parents
  • Jim,

    On the ADC side, you can potentially use a dual ADC to save on space and component count instead of using the AD9246 which is only a single.  You can look at the AD9258 or the AD9268 which is the 16-bit version.  Concerning the ADC driver, is there something that caught your interest with the AD8351?  There are newer and higher performing parts that would fit your application better.  You may want to look into the AD8366, ADL5561/62/65, AD8375/76, ADL5201/02.

    Qui

Reply
  • Jim,

    On the ADC side, you can potentially use a dual ADC to save on space and component count instead of using the AD9246 which is only a single.  You can look at the AD9258 or the AD9268 which is the 16-bit version.  Concerning the ADC driver, is there something that caught your interest with the AD8351?  There are newer and higher performing parts that would fit your application better.  You may want to look into the AD8366, ADL5561/62/65, AD8375/76, ADL5201/02.

    Qui

Children
No Data