Post Go back to editing

Questions regarding AD8351: Is there a spice model?

I'm looking for a spice model fore the AD8351. I've loooked but it doesn't seem to be posted. Does any one have one?

jim

Parents
  • Thanks for the quick reply and the infomation. I'm using this device to drive a AD9246. I'm considering drivng two of these ADCs with one AD8351 in a time interleaved system. The system has a bandwidth of 300Mhz and a gain of 3 with the ADCs at 125 Mhz. Does it make sense to use one driver for both ADCs or a driver per ADC ?

    Thanks,

    Jim

Reply
  • Thanks for the quick reply and the infomation. I'm using this device to drive a AD9246. I'm considering drivng two of these ADCs with one AD8351 in a time interleaved system. The system has a bandwidth of 300Mhz and a gain of 3 with the ADCs at 125 Mhz. Does it make sense to use one driver for both ADCs or a driver per ADC ?

    Thanks,

    Jim

Children
No Data