Post Go back to editing

ADA4960 low frequency (100kHz<f<10MHz)

I'm considering the ADA4960-1 for an ADC driver application that requires requires a fairly low frequency AC coupling (30kHz) and a maximum signal frequency of 200MHz.  The datasheet of the ADA4960-1 does not have any data for frequencies less than 10MHz.  What performance (distortion, noise) can I expect in the 30kHz - 10MHz range if input and output are capacitively coupled?

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.