ADA4960 low frequency (100kHz<f<10MHz)

I'm considering the ADA4960-1 for an ADC driver application that requires requires a fairly low frequency AC coupling (30kHz) and a maximum signal frequency of 200MHz.  The datasheet of the ADA4960-1 does not have any data for frequencies less than 10MHz.  What performance (distortion, noise) can I expect in the 30kHz - 10MHz range if input and output are capacitively coupled?