Post Go back to editing

1550 nm VCSEL driver

Hello,

I am looking for a driver for direct-modulation of a 1550 nm VCSEL (Cylindrical TO package, manufactured by Raycan).
I noticed AD product: ADN2531 and its evaluation boards: EVAL-ADN2531-NPZ , EVAL-ADN2531-NTZ.

I have the following questions that I will be grateful if you could answer:
 
1)      Is this driver suitable for the 1550 nm Raycan VCSEL? If not the optimal, Could you suggest a model more suitable for this VCSEL?

2)      What is the difference between the two evaluation boards?

3)      Is there a datasheet or some details on the evaluation boards?

4)      Can I order samples of the ADN2531 driver and of the evaluation board?

Thank you,

Amos

  • Dear Amos,

    Thank you for sharing us your questions. To better understand your questions,

    would you please send me the mentioned VCSEL laser datasheet for a review?

    Both ADN2525 and ADN2531 devices are 11.3G capable, DML drivers.

    They sink both BIAS and IMOD currents from the VCSEL laser diode.

    The major differences are based on the devices. Please see the Isupply difference below:

    ADN2525:


     
    I SUPPLY [i]

     

     

     

     
    157

     

     
    176

     

     
    mA

     

     
    V BSET = V MSET = 0 V; I SUPPLY
      = I CC + IMODP + IMODN

     

    ADN2531:


     
    I SUPPLY [i]

     

     

     

     
    55

     

     
    62

     

     
    mA

     

     
    V BSET = V MSET = 0 V

     

    Yes, you can order ADN2531 device samples and the EVB.
    Please contact ADI local sales office to get these samples.

     

    Both ADN2525 and ADN2531 datasheets are available from ADI
    public website. For example, you can have the ADN2525 from link: http://www.analog.com/en/fiberoptic/laser-drivers/adn2525/products/product.html

     

    We have application notes for these 10G LDD EVBs. Please send
    us your email contact information so that we can forward you the required EVB application
    note information.

        

    Hope these are useful to your evaluation. We are looking forward to working with you.

       

    Best Regards,

      

    Dongfeng Zhao

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.