Post Go back to editing

ADA4922-1 Offset voltage and Output Load

Hi

I am using ADA4922-1 to convert a single ended square wave of 1 KHz frequency from single ended to differential. The input square wave have an arbitrary DC offset. In order to remove the DC offset i am using a high pass filter between signal source and input of ADA4922-1. The high pass filter is a capacitor of 1uf in series and a resistor of 300K in parallel. The problem is that ADA4922-1 itself is introducing an offset of about 0.3V at the input. Even when there is no input signal, 0.3V apear at the input port while the output of ADA4922-1 is correspondingly at +/-0.3V.

Supply voltage is +/- 12V with 100 nF coupling capacitor. Both outputs have an RC low pass filter R=41 ohms, C=3.9 nF. The output drives an ADC with input impedance of 1 Gohms

Please suggest a solution to remove this DC offset. Also suggest should i add a load resistor as the ADC impedance is very high?

Thankyou & Regards

Kashef