Post Go back to editing

Is it possible to precision rectify a 1MHz signal?

For an Overcurrent detector, the present solution is a full wave bridge of MBR0530 diodes, and the forward drop of these diodes is the cause of increasing error towards the low setting.

The current signal is presented across a 5.1 ohm resistor from a 1:1000 current transformer, rectified, and compared to an adjustable and metered reference, with an AD311 comparator.

There is a 5 volt and a 9 volt supply available, and the frequency of the signal can vary from 20kHz and up to 1 MHz.

Is it possible to build a precision rectifier that runs from a single supply, and functions up to 1 MHz?

Cheers, Finn Hammer

Parents Reply Children
No Data