AD8276
Production
The AD8276/AD8277 are general-purpose, unity-gain difference amplifiers intended for precision signal conditioning in power critical applications that...
Datasheet
AD8276 on Analog.com
AD7192
Production
The AD7192 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog...
Datasheet
AD7192 on Analog.com
I need some advice on interfacing an ICP piezo force sensor from PCB Piezotronics to a microcontroller. The sensor has a low impedance output of 0-5 volts superimposed on a DC offset of 10 volts. The data must be collected in DC coupled mode for time response reasons. The signal will be low frequency, below 1 KHz. Basically what I would like to do is level shift the DC offset and send the signal into an 0-5V capable ADC with some sort of serial interface, say SPI. I cannot use an AC coupling capacitor due to the DC coupling requirement. The system will have single sided power available up to 24V, with 5V and 3.3V for other components. There are a myriad of ways to do this it seems but I have found no direct examples on the web. I was thinking of using an AD8276 unity gain difference amp with the ICP force sensor signal as the in+, 10 volts as the in-, 0 volts as the REF and sending the resulting OUT signal possibly to a AD7192 Sigma-delta ADC. We use the AD7192 currently for load cells and it works great. Does this approach sound reasonable or is there a better way. This is a new project so we are open to an suugestions
Thanks for your help.
mason100 - Moved from ADC Drivers to Differential Amplifiers and ADC Drivers. Post date updated from Wednesday, November 16, 2011 2:22 AM UTC to Thursday, July 25, 2024 8:34 PM UTC to reflect the move.
Hello Greg,
It is powered from the same supply as the inamp, or 24V according to the schematic. Actually I am glad you asked, since it just made me realize I had a small mistake in my schematic. To get the correct gain from the AD8274, you have to connect the 12k resistor to ground. I'm sorry for the confussion.
Regards,
Gustavo
Hello Greg,
It is powered from the same supply as the inamp, or 24V according to the schematic. Actually I am glad you asked, since it just made me realize I had a small mistake in my schematic. To get the correct gain from the AD8274, you have to connect the 12k resistor to ground. I'm sorry for the confussion.
Regards,
Gustavo