Post Go back to editing

ICP Piezo Force Sensor Interface to microcontroller

I need some advice on interfacing an ICP piezo force sensor from PCB Piezotronics to a microcontroller. The sensor has a low impedance output of 0-5 volts superimposed on a DC offset of 10 volts. The data must be collected in DC coupled mode for time response reasons. The signal will be low frequency, below 1 KHz. Basically what I would like to do is level shift the DC offset and send the signal into an 0-5V capable ADC with some sort of serial interface, say SPI. I cannot use an AC coupling capacitor due to the DC coupling requirement.  The system will have single sided power available up to 24V, with 5V and 3.3V for other components. There are a myriad of ways to do this it seems but I have found no direct examples on the web. I was thinking of using an AD8276 unity gain difference amp with the ICP force sensor signal as the in+, 10 volts as the in-, 0 volts as the REF and sending the resulting OUT signal possibly to a AD7192 Sigma-delta ADC. We use the AD7192 currently for load cells and it works great. Does this approach sound reasonable or is there a better way. This is a new project so we are open to an suugestions

Thanks for your help.

Thread Notes

Parents
  • Gustavo:

    I am getting a little confused on the output of the sensor. My understanding is that the signal ranges from 10 volts to 15 volts depending on the load on the sensor. As it is a piezo, the charge increases with a change in load and then drops back to a baseline value. In my mind it is like half a sine wave. In AC coupled mode, a capacitor is used to remove the DC component and the values can be read from using an ADC. I cannot use the AC coupled mode due to the time constant of the sensor in AC coupled mode. I do not think the signal is bipolar centered around the offset. I thought the AC part of the signal was simply the fast response time of the sensor. However, I could be way off on this. The sensor is a standard piezo with an charge amplifier built in.

    The mid-reference makes sense to me with regard to a bi-polar signal. I can also take care of the voltage reference as per your circuit. I was thinking it needed to be adjustable with regard to the sensor zero. I will have a stepdown voltage available so the reference will not be powered from the 24V source.

    Greg

Reply
  • Gustavo:

    I am getting a little confused on the output of the sensor. My understanding is that the signal ranges from 10 volts to 15 volts depending on the load on the sensor. As it is a piezo, the charge increases with a change in load and then drops back to a baseline value. In my mind it is like half a sine wave. In AC coupled mode, a capacitor is used to remove the DC component and the values can be read from using an ADC. I cannot use the AC coupled mode due to the time constant of the sensor in AC coupled mode. I do not think the signal is bipolar centered around the offset. I thought the AC part of the signal was simply the fast response time of the sensor. However, I could be way off on this. The sensor is a standard piezo with an charge amplifier built in.

    The mid-reference makes sense to me with regard to a bi-polar signal. I can also take care of the voltage reference as per your circuit. I was thinking it needed to be adjustable with regard to the sensor zero. I will have a stepdown voltage available so the reference will not be powered from the 24V source.

    Greg

Children
No Data