AD8276
Production
The AD8276/AD8277 are general-purpose, unity-gain difference amplifiers intended for precision signal conditioning in power critical applications that...
Datasheet
AD8276 on Analog.com
AD7192
Production
The AD7192 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog...
Datasheet
AD7192 on Analog.com
I need some advice on interfacing an ICP piezo force sensor from PCB Piezotronics to a microcontroller. The sensor has a low impedance output of 0-5 volts superimposed on a DC offset of 10 volts. The data must be collected in DC coupled mode for time response reasons. The signal will be low frequency, below 1 KHz. Basically what I would like to do is level shift the DC offset and send the signal into an 0-5V capable ADC with some sort of serial interface, say SPI. I cannot use an AC coupling capacitor due to the DC coupling requirement. The system will have single sided power available up to 24V, with 5V and 3.3V for other components. There are a myriad of ways to do this it seems but I have found no direct examples on the web. I was thinking of using an AD8276 unity gain difference amp with the ICP force sensor signal as the in+, 10 volts as the in-, 0 volts as the REF and sending the resulting OUT signal possibly to a AD7192 Sigma-delta ADC. We use the AD7192 currently for load cells and it works great. Does this approach sound reasonable or is there a better way. This is a new project so we are open to an suugestions
Thanks for your help.
mason100 - Moved from ADC Drivers to Differential Amplifiers and ADC Drivers. Post date updated from Wednesday, November 16, 2011 2:22 AM UTC to Thursday, July 25, 2024 8:34 PM UTC to reflect the move.
Gustavo:
Thank you for your detailed answer. I have a couple of questions about your schematic. In your comments you say that AD8276 is used to drive the reference pin of the AD8226 to mid reference. What value are you considering mid-reference? To me it means the mid value between what would be adjusted with the Radj resistor. For example, if I adjust the reference from 10-10.2 volts then mid-reference would be 10.1 volts. Is this correct? Then the value of Vref would be 10.1? volts?
I am going to incorporate this circuit into my design. Do you have any pointers for the Vref voltage source? I did a quick scan of your web site and there are many 10V reference sources but all of them seem to be fixed at 10.0 volts. Sorry if this is a basic question but I am much more comfortable with the digital side of circuits than the analog.
Best regards,
greg
Gustavo:
Thank you for your detailed answer. I have a couple of questions about your schematic. In your comments you say that AD8276 is used to drive the reference pin of the AD8226 to mid reference. What value are you considering mid-reference? To me it means the mid value between what would be adjusted with the Radj resistor. For example, if I adjust the reference from 10-10.2 volts then mid-reference would be 10.1 volts. Is this correct? Then the value of Vref would be 10.1? volts?
I am going to incorporate this circuit into my design. Do you have any pointers for the Vref voltage source? I did a quick scan of your web site and there are many 10V reference sources but all of them seem to be fixed at 10.0 volts. Sorry if this is a basic question but I am much more comfortable with the digital side of circuits than the analog.
Best regards,
greg