AD8276
Production
The AD8276/AD8277 are general-purpose, unity-gain difference amplifiers intended for precision signal conditioning in power critical applications that...
Datasheet
AD8276 on Analog.com
AD7192
Production
The AD7192 is a low noise, complete analog front end for high precision measurement applications. It contains a low noise, 24-bit sigma-delta (Σ-Δ) analog...
Datasheet
AD7192 on Analog.com
I need some advice on interfacing an ICP piezo force sensor from PCB Piezotronics to a microcontroller. The sensor has a low impedance output of 0-5 volts superimposed on a DC offset of 10 volts. The data must be collected in DC coupled mode for time response reasons. The signal will be low frequency, below 1 KHz. Basically what I would like to do is level shift the DC offset and send the signal into an 0-5V capable ADC with some sort of serial interface, say SPI. I cannot use an AC coupling capacitor due to the DC coupling requirement. The system will have single sided power available up to 24V, with 5V and 3.3V for other components. There are a myriad of ways to do this it seems but I have found no direct examples on the web. I was thinking of using an AD8276 unity gain difference amp with the ICP force sensor signal as the in+, 10 volts as the in-, 0 volts as the REF and sending the resulting OUT signal possibly to a AD7192 Sigma-delta ADC. We use the AD7192 currently for load cells and it works great. Does this approach sound reasonable or is there a better way. This is a new project so we are open to an suugestions
Thanks for your help.
mason100 - Moved from ADC Drivers to Differential Amplifiers and ADC Drivers. Post date updated from Wednesday, November 16, 2011 2:22 AM UTC to Thursday, July 25, 2024 8:34 PM UTC to reflect the move.
Gustavo:
In answers to your questions:
1) The offset is determined by the sensor electronics. The sensor itself is a piezo charge output sensor with a built in mosfet amplifier. The amplifier converts the charge output of the piezo sensor to a low impedance voltage output. The impedance is listed as less than 100 ohms. The supply voltage to the sensor 18-24 Volts constant current to maintain a linear response. I am not sure if the signal is radiometric but regardless supply voltage needs to be 24Volts which will result in an offset of 10Volts and a signal range of 0 to 5 volts.
2) This is a hard question to answer as the range could change depending on the sensor chosen and test being run. As a simple answer, resolution of 0.1mv out of a 5V signal would be great. However, in reality this resolution would only be needed for a smaller range say to 1V and then switch to 1mv for full scale readings. The ideal system would incorporate digital control to adjust range and resolution as needed.
3) We have not chosen a specfic sensor but ICP is an acronym for "integrated circuit piezoelectric", and is a registered trademark of PCB Piezotronics. This is also similar to IEPE which is the standard for piezoelectric transducers and is also an acronym for "Integrated electronics piezo electric".
Thanks for your help
Greg
Gustavo:
In answers to your questions:
1) The offset is determined by the sensor electronics. The sensor itself is a piezo charge output sensor with a built in mosfet amplifier. The amplifier converts the charge output of the piezo sensor to a low impedance voltage output. The impedance is listed as less than 100 ohms. The supply voltage to the sensor 18-24 Volts constant current to maintain a linear response. I am not sure if the signal is radiometric but regardless supply voltage needs to be 24Volts which will result in an offset of 10Volts and a signal range of 0 to 5 volts.
2) This is a hard question to answer as the range could change depending on the sensor chosen and test being run. As a simple answer, resolution of 0.1mv out of a 5V signal would be great. However, in reality this resolution would only be needed for a smaller range say to 1V and then switch to 1mv for full scale readings. The ideal system would incorporate digital control to adjust range and resolution as needed.
3) We have not chosen a specfic sensor but ICP is an acronym for "integrated circuit piezoelectric", and is a registered trademark of PCB Piezotronics. This is also similar to IEPE which is the standard for piezoelectric transducers and is also an acronym for "Integrated electronics piezo electric".
Thanks for your help
Greg