Post Go back to editing

Queries on CN-0105: drive ckt for AD7626

Hi,

I am new to using ADCs. I have 3 different kinds of signals which I need to sample and process. The frequencies are 1KHz, 10KHz & 100 Khz, and all are single-ended. I want around 100 samples per cycle, with about 12-14 bit accuracy. So I have chosen AD7626 (16-bit) with 10MHz sampling rate. When I sample the highest frequency signal (100KHz), I will run the ADC with 10MHz clock, and when I receive the other signals, I will bring down the sampling rate by a factor of 10 & 100 accordingly. How is the idea?

In addition, I want to use the ADA4932 for driving the AD7626 rather than ADA4899. In CN-0105, it is mentioned that ADA4899 is the recommended driver at lower frequencies. I want to know what are the issues with ADA4932 at lower frequencies (1KHz - 100KHz). I like ADA4932 since it is a single chip solution. If it is input referred noise, I am okay with it, since some amount of noise is not much of an issue with me.

I have a third query. It will be difficult for me to generate +7.25V required for the +Vs power of ADA4932. So I am planning to use +5V instead. I want to know what is the effect of this. Will it just bring down the dynamic range of the output. I can take care of that by reducing the input swing.

thanks and regards,

rajesh

Thread Notes

  • Hi rajesh,

    ADA4932 is recommended for higher frequencies because of its excellent distortion performance at these higher frequencies. You are correct that at lower frequencies, ADA4899 has better noise performance compared to ADA4932. However, it doesn't mean that ADA4932 can't be used for lower frequencies. You can use the ADI Diff-Amp Calculator to simulate the ADA4932 and see if its overall noise performance is acceptable in your design. You are also correct that by reducing the +Vs from +7.25 to +5V reduces the dynamic range of the output. You can verify that using the ADI Diff-Amp Calculator.

    Regarding your concern on the ADC, you may contact the Precision ADC Community. They will be more than willing to help you on your ADC needs.

    Thank you for considering ADI products in your design.

    Hope this helps.

    Neil

  • Hi Rajesh,

    I co-wrote the CN-0105, I'd like to make a few additional comments here. As for the ADA4899 vs.ADA4932, as Neil mentioned the ADA4932 provides better high frequency performance. The ADA4899 does offer better distortion performance at lower freq (~<1MHz). As for supply voltages, yes you can use lower supplies for the ADA4932 as long as you stay within the operating range (input and output) of the device and if you have smaller signals that should not be an issue.

    As for the sampling questions, I spoke with our PulSar apps engineer and she had the following to say.

    "On the sampling question, I don’t see an issue with his proposal. He could continue to sample at 10MHz for all of the input frequencies if he wishes. Maybe there is a particular reason he wants to slow the sampling for the lower input tones?

    One thing I would say, if he only needs 12/14 bits and the max bandwidth of his signal is 100kHz, the AD7626 is probably overkill – the AD7980 would probably do the job also or even the AD7944 at 14 bits. Possibly the LVDS interface on the AD7626 is a requirement?"

    I hope this helps answer your questions, let me know if there is anything else I can do to help.

    Regards

    JohnA

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.