ADA4960-1
Recommended for New Designs
The ADA4960-1 is a high performance, differential amplifier optimized for RF and IF applications. It achieves better than 63 dB IMD3 performance for frequencies...
Datasheet
ADA4960-1 on Analog.com
The ADA4960 datasheet mentions:
"The buffered inputs of the ADA4960-1 isolate the gain-setting
resistor (RG) from the signal inputs, maintaining a constant 10 kΩ
input resistance, easing matching and input drive requirements."
Does this affect the behaviour of the feedback resistor? Can I use several gain resistors switched by a coax relay?
What is the best way to implement 2 or 3different gain settings?
mason100 - Moved from ADC Drivers to Differential Amplifiers and ADC Drivers. Post date updated from Sunday, March 17, 2013 3:16 AM UTC to Thursday, July 25, 2024 8:35 PM UTC to reflect the move.