ADA4960-1
Recommended for New Designs
The ADA4960-1 is a high performance, differential amplifier optimized for RF and IF applications. It achieves better than 63 dB IMD3 performance for frequencies...
Datasheet
ADA4960-1 on Analog.com
The ADA4960 datasheet mentions:
"The buffered inputs of the ADA4960-1 isolate the gain-setting
resistor (RG) from the signal inputs, maintaining a constant 10 kΩ
input resistance, easing matching and input drive requirements."
Does this affect the behaviour of the feedback resistor? Can I use several gain resistors switched by a coax relay?
What is the best way to implement 2 or 3different gain settings?
mason100 - Moved from ADC Drivers to Differential Amplifiers and ADC Drivers. Post date updated from Sunday, March 17, 2013 3:16 AM UTC to Thursday, July 25, 2024 8:35 PM UTC to reflect the move.
Hi, Bernhard.
ADA4960-1 has dedicated pins for the gain setting which makes it easier to configure the desired gain from a range of 0dB to 18dB by using a single resistor. This feature eliminates the use of two resistors, as Rg and Rf, to configure the gain which is mostly done in conventional op amps. You may refer to page 15 of the datasheet for more details about this.
Yes, you can use a relay to set the gain but there are disadvantages like "OFF"-state leakage currents that flow through the switching device, high "ON"-state voltage drop and high power dissipation that you have to consider in using it. As alternative to this, you may use ADI's multiplexers for a more controlled signal path and are in smaller package. You may look at this link and also you may refer to this tutorial for multiplexers.
Hope this helps. Let me know if you have other concerns.
Thanks,
Anna
Hi, Bernhard.
ADA4960-1 has dedicated pins for the gain setting which makes it easier to configure the desired gain from a range of 0dB to 18dB by using a single resistor. This feature eliminates the use of two resistors, as Rg and Rf, to configure the gain which is mostly done in conventional op amps. You may refer to page 15 of the datasheet for more details about this.
Yes, you can use a relay to set the gain but there are disadvantages like "OFF"-state leakage currents that flow through the switching device, high "ON"-state voltage drop and high power dissipation that you have to consider in using it. As alternative to this, you may use ADI's multiplexers for a more controlled signal path and are in smaller package. You may look at this link and also you may refer to this tutorial for multiplexers.
Hope this helps. Let me know if you have other concerns.
Thanks,
Anna