Post Go back to editing

AD8475 introduces too much noise, any suggestions?

I'm driving an LTC2440 24 bit sigma delta ADC with an AD8475 funnel amplifier. If I short the ADC inputs together I measure about 7 counts RMS noise, which is about 2uV RMS. This matches my expectation and the figures quoted on the ADC datasheet for a system with a 10Hz to 1kHz bandwidth. My problem is that when I drive the ADC through the AD8475 I measure 105 counts RMS of noise, which is over 25uV RMS.

Can anyone suggest a way of improving on this?

Thread Notes

  •      Hello  Oliver,

         Perhaps you could try throttling down the AD8475's bandwidth with a cap directly across the ADC differential input (after the 47 ohm resistors).  0.1uF might be a good starting point. The AD8475 is built for 4 MS/s @ 18 bit operation, so it may allow through some high-frequency noise that your ADC can't handle.  The LTC2440 has a neat resolution vs. speed tradeoff feature, but ADCs are not always 100% resistant to out-of-band noise.

         Best regards,

         Bob

  • Thanks Bob,

    I tried a 10nF cap across the ADC inputs and saw a great improvement. It gave a slightly mysterious DC shift with oversampling ratio, so I also tried two 10nF caps to ground. This gives me 14 counts RMS noise with no DC effects, so I'm a happy bunny!

    Oliver

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.