Post Go back to editing

ADA4930-1 Input DC Adjustment from DAC

Dear Sir/Madam,

I am planning on using AD8336, ADA4930-1 and AD9681.

AD8336 to ADA4930-1 is DC coupled with unipolar signal that has DC offset.

The unipolar signal is connected to the non-inverting input of the ADA4930-1.

What options are available to adjust the unipolar signals DC offset so that it is within the

input common mode range of the ADA4930-1 (0V3 to 1V2) ?
The adjustment would need to be +- using
AD5516.


Regards Grant

Thread Notes