Dear Sir/Madam,
I am planning on using AD8336, ADA4930-1 and AD9681.
AD8336 to ADA4930-1 is DC coupled with unipolar signal that has DC offset.
The unipolar signal is connected to the non-inverting input of the ADA4930-1.
What options are available to adjust the unipolar signals DC offset so that it is within the
input common mode range of the ADA4930-1 (0V3 to 1V2) ?
The adjustment would need to be +- using AD5516.
Regards Grant