Post Go back to editing

ADL5201 Common Mode Input Voltage

Hi,

In table 1 of the ADL5201 data sheet it states that the input can be +/-10V p-p if the attentaution is set at -11.5db.

Yet, in table 2 the absolute maximum VIN+ and VIN- specifications provided don't tally with the above figure.

Does anyone know what the true VN+ and VIN- Maximum/Minimum ranges are?

Thanks Anthony

Thread Notes

Parents
  • Hi,

    I still don't get the full picture.

    With a common mode voltage of +1.5 V, for example,  the negative is allowed to swing down to -1.2 V (presumably). resulting in a  2.7 V peak swing. At the same time, for example, the positive input can swing up to +3.6 V, resulting in a 2.1 V peak for a total of 4.8 V p-p (not 10.8V as per the data sheet).

    Assuming that the positive input could also swing by +2.7 V, the total would now be 5.4 V p-p. And, assuming the 10.8 V specification quoted is with s source impedance of 150 Ohm (the impedance of the device) then the 10.8 V figure comes into the picture.

    But, there are a lot of assumptions in the above.

    Is there a simpler explanation for how the 10.8V p-p is derived?

    Regards Anthony

Reply
  • Hi,

    I still don't get the full picture.

    With a common mode voltage of +1.5 V, for example,  the negative is allowed to swing down to -1.2 V (presumably). resulting in a  2.7 V peak swing. At the same time, for example, the positive input can swing up to +3.6 V, resulting in a 2.1 V peak for a total of 4.8 V p-p (not 10.8V as per the data sheet).

    Assuming that the positive input could also swing by +2.7 V, the total would now be 5.4 V p-p. And, assuming the 10.8 V specification quoted is with s source impedance of 150 Ohm (the impedance of the device) then the 10.8 V figure comes into the picture.

    But, there are a lot of assumptions in the above.

    Is there a simpler explanation for how the 10.8V p-p is derived?

    Regards Anthony

Children
No Data