Post Go back to editing

ADL5201 Common Mode Input Voltage

Hi,

In table 1 of the ADL5201 data sheet it states that the input can be +/-10V p-p if the attentaution is set at -11.5db.

Yet, in table 2 the absolute maximum VIN+ and VIN- specifications provided don't tally with the above figure.

Does anyone know what the true VN+ and VIN- Maximum/Minimum ranges are?

Thanks Anthony

Thread Notes

Parents
  • Hi Anthony,

                       The 10.8 V p-p swing mentioned in Table 1 is the  maximum AC signal swing allowed when the amplifier is set to minimum gain. The input  common mode voltage is 1.5 V. ( see Table1)

    The V+ - V- voltages listed in table 2, are the Absolute Maximum DC voltage levels that should be applied to the input pins of the ADL5201.

Reply
  • Hi Anthony,

                       The 10.8 V p-p swing mentioned in Table 1 is the  maximum AC signal swing allowed when the amplifier is set to minimum gain. The input  common mode voltage is 1.5 V. ( see Table1)

    The V+ - V- voltages listed in table 2, are the Absolute Maximum DC voltage levels that should be applied to the input pins of the ADL5201.

Children
No Data