Post Go back to editing

CN0271 : +2.5V -connection at AD8476

Hi there,

I'm creating a system to measure temperatures. It's based on the CN0271 except the ADC. I've chosen a faster one. I'm wondering why the negative input of the AD8476 is tied to +2.5 V. Is this done to be able to measure negative temperatures? Like an offset to 2.5V ?

Thanks a lot

Thread Notes

Parents
  • Hi Daniel,

    AD7990's differential input voltage range condition is +/-REFIN/GAIN. In CN-0271 REFIN(+) = +2.5v, REFIN(-) = GND. Meaning the differential input of the ADC is within +/-2.5V. 

    The transfer function of the differential amplifier is:

    Since Rf/Rg = 1, then,

    Moving on, for the AD8495 the full scale output voltage of the device when in single supply mode is 0.025V to 4.9V. 

    So the Vout,dm of the differential amplifier -2.475V to 2.4V, which suits the conditions of the differential input of ADC.


    Let me know if you have any clarifications.

    Regards,

    Goz

Reply
  • Hi Daniel,

    AD7990's differential input voltage range condition is +/-REFIN/GAIN. In CN-0271 REFIN(+) = +2.5v, REFIN(-) = GND. Meaning the differential input of the ADC is within +/-2.5V. 

    The transfer function of the differential amplifier is:

    Since Rf/Rg = 1, then,

    Moving on, for the AD8495 the full scale output voltage of the device when in single supply mode is 0.025V to 4.9V. 

    So the Vout,dm of the differential amplifier -2.475V to 2.4V, which suits the conditions of the differential input of ADC.


    Let me know if you have any clarifications.

    Regards,

    Goz

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.