Post Go back to editing

Common Mode Question (AD8138 part, single supply)

Good afternoon,

I am working with the AD8138 part and am having some issue with the common mode reference in my simulations.  Due to constraints on the board, we are only able to use a single supply to operate from, the AD8138 has been a relatively good part in the past for me, although I've never used it without a dual supply. 

I might be missing something obvious here, or perhaps the model that I have doesn't support a single supply applications very well.  Thinking I was setting this up wrong, I copied the schematic from Figure 42 from the datasheet.  The problem I am seeing is that the output voltage levels are ~ 2.1V above the common mode set point.  (i.e., set the common mode to 2.5V, the Vpos and Vneg are sitting at 4.65V.  For an input I am applying a 100kHz sine wave with a DC offset of 0.5V, and a peak-peak amplitude of 0.5V. 

I also ran DC sweeps on the same circuit to see where the outputs were in relation to the common mode reference point.  They are always ~ 2V greater than the common mode set point.  This is not a complicated circuit, I don't think I'm doing anything wrong with the setup.  What made me start suspecting the model is if I set the common mode down to around 500mV, the AD8138 current draw sky rockets up to 350MA (not milli, but MEGA).  If I run the same sweep with a -5V rail, it performs as expected.

Has anyone else reported any strange issues with the common mode at the outputs when using a single supply?

As always, thanks for your time,

Dave

Parents Reply
  • This question was never answered.  Has anyone looked into why the common mode voltage doesn't follow the output while using a single supply?  Is this a real behavior of the AD8138? 

    As I stated above, the AD8139 was a work around for someone else, but is that really a work around?  The AD8139 is a different part, and if your intention is to use the AD8138 this might not be good. 

    Dave

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.