Hi
Please provide input (common mode) voltage range and output voltage range min and max for following opamps
LT809 supply +5V, -5V
LT6230-10 supply +5V, -5V
Datasheets' values are so confusing for these two parts. it is not clear from datasheets of these parts that what is the input and output voltage ranges. I am looking for something as clear as like attached image below.This screenshot is from a TI opamp datasheet. It's so clearly mentioned in TI datasheets but its always very confusing for LT opamps datasheets. Please help me with input voltage range and output voltage range for LT809 and LT6230-10
Thanks
Santosh