Post Go back to editing

AD8129 noise improvement

I used AD8129 as a differential amplifier in my project. 

My specifications are meet the criteria except for NOISE.

Is there any way to improve the noise for AD8129?

Please teach me how to improve the noise of AD8129.

Parents
  • Hi Jayson042907,

    Can you share more details about your schematic configuration? How much noise are you measuring on the AD8129 that you'd like to reduce the noise?

    Regards,

    Hooman

  • Hello Hooman,

    Sorry for the late reply.

    I used the AD8129 as a differential amplifier with the attenuator circuit of 4M ohms & 40k ohms.

    My criteria for noise is 0.65mV but the actual noise that I measured is 1.2mV.

    Do you have any idea how to reduce the noise further?

    Please teach me how to calculate the noise for AD8129.

  • Hello again,

    I forgot to mention.

    Of course lowering the values of your attenuation is another way to improve the AD8129 output noise, if the buffer after the attenuator idea above is not feasible.

    If your application allows a much lower impedance 100:1 attenuation, like 100k and 1k, the noise will be lower by about 10x factor, as described below:

    1) 1k noise: 4.07nV/RtHz

    2) AD8129 input referred current noise RTI: 1pA/RtHz * 1k= 1nV/RtHz

    3) AD8129 input referred voltage noise RTI: 4.6nV/RtHz

    So now, you'd be limited by the AD8129 voltage noise and not by the attenuator thermal noise or the AD8129 input current noise flow through the attenuator impedance.

    The noise reduction will be from ~40nV/RtHz to ~4.6nV/RtHz when you drop the attenuator resistors by a factor of 40x from 40k to 1k.

    Regards,

    Hooman

  • Hello Hooman,

    Thank you for the suggestion.

    I prefer your first suggestion to add a buffer after the attenuator. Because the attenuator is already fixed and the only thing need to change is the voltage gain(Rg & Rf) of the AD8129.

    I will use a source follower FET transistor configuration as a buffer.

    Do you think it is good idea? Please give me advice.

    It is my first time to design a project regarding the AD8129 application.

    Thanks & best regards,

    Jayson

  • Hi Jayson,

    Regarding a JFET follower before the AD8129 to reduce AD8129 input bias current induced noise:

    I assume you have a DC coupled signal path.

    To implement such a discrete JFET buffer when you're DC coupled, I think you'd have to get creative with matching JFET VGS, etc. as described in this article:

    https://www.planetanalog.com/buffer-amplifier-design/

    This may not be a practical approach.

    You may be better off just using a low noise, low input bias current integrated buffer like ADA4891-1 or ADA4610-1 instead to avoid having to deal with the DC offset problem.

    Hope this helps.

    Regards,

    Hooman

  • Hi Jayson,

    Regarding AD8129 and your need to reduce noise:

    If you're attenuating the input signal, are you sure AD8129 is the right part to use? AD8129 is only stable for gains of 10V/V or higher. AD8130 can be used at a gain of 1V/V. So, I can't quite understand why the need for attenuation if you're running the AD8129 at 10x gain or higher?

    Furthermore, do you know what signal bandwidth you need? I'd guess that that your 100:1 attenuator (4M, 40k) is band-limited to 1MHz or less. If so, you'd probably benefit from reducing the bandwidth you get from AD8129 (or AD8130?). I've done that in the zip file attached below where a 5pF cap across RF has reduced the overall bandwidth to around 1MHz to reduce the output noise. You could manipulate the circuit yourself to see the effect.

    AD8129 LTspice response 9_18_19.zip

    Note: The AD8129 pspice model from the web, which I've imported into LTspice, does not model the device's noise as shown in the model's text / comments lines.

    Regards,

    Hooman

  • Hello Hooman,

    I have a question regarding JFET follower. JFET follower has a unity voltage gain so, Vin is almost equal to Vout.

    But in my actual experiment, Vin is not equal to Vout. When my Vin1 = 0.2V , the Vout1 = 1.201V. The actual Vgs value = -1.01V.  While Vin2 = 0.0V, the Vout2 = 1.01V. Therefore, Vout = Vin - Vgs.

     Is it correct? How can I make Vin = Vout?

    I cannot upload the picture of my circuit. I hope you understand my circuit.

    I used LS5911 IC JFET. I connect +9.5V at the Drain ( pin 6 & pin 2). I input Vin1 = 0.2V to LS5911 pin 7 and Vin2 = 0.0V to LS5911 pin 3. I connect RS = 2K ohms to the LS5911 pin5.

    Then, I connect a current source (BJT) at the end of RS resistor.

    I used PMBT2222A transistor as a current source. I used RB = 51K connected to the ground at the other end. I connect LED (Vf = 1.2V) to PMBT2222A pin 1  and the other end is connected to -9.5V supply. I connect RE = 500ohms to PMBT2222A pin 2 and the other end of the RE is connected to -9.5V supply.

    My +Vin of AD8129 is connected to LS5911 pin 1 while the -Vin of AD8129 is connected to LS5911 pin 5.

    Best regards,

    Jayson

  • Hello Hooman,

     Thank you very much for your suggestion.

     My BW requirement is 75MHz.

     I will try it after I finish my experiment in JFET follower.

     I'm still debugging the JFET follower.

  • Hi Jayson,

    If you convert your jpg picture to a zip file you can upload onto EZ.

    Regards,

    Hooman

  • Hi Jayson,

    Regarding the JFET buffer you're trying to put together:

    As I already mentioned on Sept. 17, a single transistor JFET will not function well as a DC coupled voltage follower due to non-zero VGS. That's why in this article they explain how to use two matched JFET's to eliminate this offset:

    https://www.planetanalog.com/buffer-amplifier-design/

    So, I recommended an off-the-shelf buffer may be the way to go.

    BTW, getting 75MHz out of your 100:1 attenuator may need some careful compensation because of the resistor / trace capacitances. A stray capacitance of 0.5 fF is enough to jeopardize this frequency with 4M resistance, unless you manage to compensate properly.

    Regards,

    Hooman

  • Hello Hooman,

    Do you have any idea regarding 1/f noise of AD8129?

    I cannot find it in datasheet.

    I already add JFET follower in my circuit but the noise becomes bigger.

    Regards,

    Jayson

  • Hello Hooman,

    My zip file is already expire.

    I try .rar file but still cannot upload my circuit.

    Best regards,

    Jayson

Reply Children
  • Hi Jayson,

    You can also attach an acrobat / pdf file here, if you can convert to pdf?

    Regards,

    Hooman

  • Here is a test to see if I can attach a jpg file?

    If the image of a key board shows up, then yes you can attach a jpg file a well.

    Hooman

  • Here are the noise plots of AD8129:

    The lower plot is incorrectly shown as "Current Noise Density". I've corrected it to read "Voltage Noise Intensity" instead.

    Operating at up to 75MHz, per your requirement, you'd most likely not be limited by 1/f noise but rather by flat-band noise.

    Regards,

    Hooman

  • Hello Hooman,

    I attached my actual circuit.PDF

    Can you teach me how to compute the noise per stage?

    I want to learn how to compute it and what are the parameters need to consider in design.

    Thank you very much.

    Best regards,

    Jayson

  • Hi Jayson,

    Here is what I did:

    1. Took your circuit and simulated it with LTspice.

    2. Since the AD8129 Pspice model does not include noise, I added the input referred input noise voltage, and input noise current (2 places) sources.

    3. I verified your JFET amplifiers functionality using Transient Simulation.

    4. I used LTspice to predict the output noise under two different conditions:

    a) With your JFET buffers in place including the 100:1 attenuator.

    b) With your JFET buffers bypassed and the 100:1 attenuator tied to AD8129 inputs.

    I found that with JFET buffers in place, I measure a much lower output noise density (371nV/RtHz) vs. the case where the 100:1 attenuator is tied to the AD8129 inputs (675nV/RtHz).

    I've shown the noise density plots for these two cases below for comparison:

    Here are the simulation files included:

    ad8129 EZ JFET Noise LTspice 10_3_19.zip

    So, simulations show the opposite of what you found; the JFET buffers do reduce noise. In fact, the simulation difference is exactly the 1pA/RtHz device noise * 40k * Gain, on each input.

    There is an improvement in bandwidth using simulation with the JFET buffers, which may be responsible for you measuring higher noise? Please double check in case you're measuring the noise using time-domain?

    Regards,

    Hooman

  • Hello Hooman,

     May I asked if the simulation includes the noise generated by the FET (LS5911) & PMBT2222A?

     Is it possible that the noise is caused by the transistor?

     My set-up in measuring noise is I short the (+/-) inputs and measured the output by the Oscilloscope (with BW limit = 20MHz). 

    Best regards,

    Jayson

  • Hi Jayson,

    To answer your questions:

    1. Discrete Noise: Yes, the simulation includes all noise sources, including the JFET and the NPN. However, you're dominated by the 40kohm resistor thermal noise (26nV/RtHz) at the Source of the JFETs.

    2. Xsistor Noise: No, the JFET noise (4nV/RtHz) does not factor into this, again because the 40kohm input attenuator noise dominates at 26nV/RtHz. Nor does the NPN noise because there is no gain from the NPN base to its collector (because the collector is looking to the low impedance of the JFET source).

    3. Time-Domain Measurement: With a 20MHz bandwidth, LTspice shows JFET buffered output noise of 1.47mV_RMS (or 9.7mVpp assuming 6.6x factor). That's vs. 780uV_RMS for the 100:1 directly interfacing the AD8129!

    The main reason for what you're measuring can be seen in the plot below where with the JFET's buffers in place, you're extending your circuit's BW from 670kHz to 18MHz! The most likely reason for the low bandwidth with the 100:1 attenuator directly interfacing with AD8129 is the input capacitance of the AD8129 lowering your frequency response. With the JFET buffers in place, you've eliminated this RC pole because of the lower Gate capacitance of the JFET's.

    So, the JFET circuit will have higher bandwidth and thus will measure noisier on the scope. For a true comparison, you must roll-off the bandwidth of the JFET setup to match the un-buffered setup.

    Regards,

    Hooman

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.