Post Go back to editing

AD826 heats up

At the moment, our department has released a filter circuit board, one of the main components of which is the AD826.
www.analog.com/.../AD826.pdf
In our circuit, the power is from a 30V block, with a midpoint of 15V. Scheme in attachment.
Operats. the amplifier heats up significantly, somewhere 55-60 degrees. The current consumption amounted to ~ 25mA, which is extremely higher than the stated 7.5mA per channel.
It was also decided to check the AD826 outside the circuit - pulled all the entrances to the ground, 28V power supply. The current consumption is 28 mA.

PS: In the same scheme, the AD823 operational amplifier consumes current like AD826 not heat up at all.

7026.Attachment.zip

Edit Notes

Attachment uploaded
[edited by: timurtemirkhanov@mail.com at 8:21 PM (GMT 0) on 27 May 2019]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.