Post Go back to editing

AD8215 Negative Current

Good day,

Can the AD8215 handle a negative sense current, i.e. what is the maximum negative differential voltage the AD8215 can handle between the IN+ & IN- pins?  I could not find a clear answer in the datasheet.

Application:

I'm using the AD8215 to sense charge current of Li-Ion battery, however when not charging, there will be a small reverse current to keep the MCU alive.  I don't need to measure this current, I just need to know that the AD8215 is OK with it, i.e. what the electrical limits are.

Best regards,

Rean Bootsma

Parents
  • Hi Rean, 

    Table 2 (Absolute Maximum Ratings) in the AD8215 datasheet indicates that you should stay within 0.5V for differential input and -3V to 68V for continuous common-mode voltage. 

    How small is the reverse current? Let me know and I can try to confirm whether the AD8215 can handle it. 

    Thanks, 

    Kris

Reply
  • Hi Rean, 

    Table 2 (Absolute Maximum Ratings) in the AD8215 datasheet indicates that you should stay within 0.5V for differential input and -3V to 68V for continuous common-mode voltage. 

    How small is the reverse current? Let me know and I can try to confirm whether the AD8215 can handle it. 

    Thanks, 

    Kris

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.