I am looking for the theta JB value for PNs: AD828ARZ and AD7547LRZ-ND. Previously I was given the Psi JB I would also like the theta JB.
Thanks,
Sam
KCC Quizzes AQQ303 about the radius of a circle
1. Quote of the month: "When I die, I want to die like my grandfather who died peacefully in his sleep. Not screaming like all the passengers in his car" - Will Rogers
2. Quiz AQQ304 about finding the radius of a circle
Good luck, and try to be
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
AD828
Production
The AD828 is a low cost, dual video op amp optimized for use in video applications which require gains of +2 or greater and high ouput drive capability...
Datasheet
AD828 on Analog.com
AD7547
Not Recommended for New Designs
The AD7547 contains two 12-bit current output DACs on one monolithic chip. Also on-chip are the level shifters, data registers and control logic for easy...
Datasheet
AD7547 on Analog.com
I am looking for the theta JB value for PNs: AD828ARZ and AD7547LRZ-ND. Previously I was given the Psi JB I would also like the theta JB.
Thanks,
Sam
Hi,
Let me look into this. Thanks!
Regards,
Goz
Hi samshoe,
AD7547LRZ-ND Rjb: 27.8°C/W based on JEDEC 2s2p thermal test board in a JEDEC Rjb test environment.
Cheers,
Ivan
Hi,
Theta-Jb of AD828ARZ is 117 C/W. Thanks for the inquiry.
Regards,
Goz