Post Go back to editing

Battery measuring by AMP03 then muxing to NI A/D


Hi,

I designed system thats monitoring batteries discharging.

There are a lot of batteries sampled by AMP03 (Unity gain, diff. amp) then transfered via 2 analog 32-1 MUX (ADG732) and analog MUX 2-1 (ADG1219) and finally driven through the another unity gain amp to NI A/D in the PC.

After some months of working the battery sample amps started to burn up at random order.

May I miss anything in the design, espessialy in AMP-MUX interface?

Thanks

Parents
  • Harry,

    Thank you for your response.

    The AMP03 is not Instrumental Amp, but precision unity gain diff amp.

    you can see the whole datasheet here http://www.analog.com/en/products/amplifiers/specialty-amplifiers/current-sense-amplifiers/amp03.html

    There are internal resistors inside the component. I connected the AMP like described in application circuits:

    What happens sometimes is that the mux input (connected to AMP03 output) is stuck in -0.5V, I suppose that's clamped by internal diode.

    I tried to add a series resistor between Amp and MUX (100R, 1K, 10K)

    I tried to connect Amp like a summing Amp (E1=E2=Battery => gain = 2) and on output I put voltage divider (two 10K resistors)

    So that's working, but when I connected it to MUX I get -0.5V in the MUX input, WHY?

    Thanks again,

    Alex

Reply
  • Harry,

    Thank you for your response.

    The AMP03 is not Instrumental Amp, but precision unity gain diff amp.

    you can see the whole datasheet here http://www.analog.com/en/products/amplifiers/specialty-amplifiers/current-sense-amplifiers/amp03.html

    There are internal resistors inside the component. I connected the AMP like described in application circuits:

    What happens sometimes is that the mux input (connected to AMP03 output) is stuck in -0.5V, I suppose that's clamped by internal diode.

    I tried to add a series resistor between Amp and MUX (100R, 1K, 10K)

    I tried to connect Amp like a summing Amp (E1=E2=Battery => gain = 2) and on output I put voltage divider (two 10K resistors)

    So that's working, but when I connected it to MUX I get -0.5V in the MUX input, WHY?

    Thanks again,

    Alex

Children
No Data