Post Go back to editing

Lowpass filter for LTC6363

I'm trying to add a 1 pole RC filter with a 20kHz cutoff upstream of the LTC6363 as an anti-alias filter. My configuration is like this:

https://tools.analog.com/en/adcdriver/#adc=LTC2512-24&cext=3e-9&driver=LTC6363&frequency=20000&gain=1&inputSettlingChart=2&multiplexed=false&nTab=1&oss=false&rext=30&rf=1050&sTab=1&samplingRate=819000&showAdcVariant=false&showDriverVariant=false&sourceType=1&tab=1&thd=200&topology=1&vSupplyNeg=-1.3&vSupplyPos=6.3&vref=5&wbNoise=0

This is for audio frequency input signals and I'll be doing a 16x or 32x decimation factor to provide additional anti-alias performance.

According to LTSPICE I can add a 30nF capacitor as shown:

...and this gives me the magnitude response I'm after, but it adds a ton of noise @ 380kHz which I assume will alias into my input signal. If there's a more optimal solution please advise! 

Parents Reply Children
No Data