I ordered DC427B Eval Board which uses LTC1968. I wanted to know If I can connect the output from LTC1968 directly to a Analog Pin of microcontroller. The output current of LTC1968 is 10mA; I was able to measure the voltage directly from the output using microcontroller but I wanted to make sure that I am not creating any sort of stress on the LTC1968.
I tried using a voltage follower between the output and the microcontroller, and the signal wasn't looking good.
DC427B-C: https://www.digikey.com/en/products/detail/analog-devices-inc/DC427B-C/4927157
LTC1968 datasheet: https://www.analog.com/media/en/technical-documentation/data-sheets/1968f.pdf
In addition, can you recommend another sine wave RMS to DC converter that works for a 200kHz sine wave signal. I have chosen LTC1968 but if there is another one with better performance, I would like to test it.
I hope to hear your response.