Hello, the LTC6400 has several pins for the V + (Pins 1, 3, 10) and V– (Pins 4, 9, 12, 17). The question is: Do they all need to be connected or just one pin for V + and one pin for V- would be enough. The question arises from a need for PCB design.
Hello, the LTC6400 has several pins for the V + (Pins 1, 3, 10) and V– (Pins 4, 9, 12, 17). The question is: Do they all need to be connected or just one pin for V + and one pin for V- would be enough. The question arises from a need for PCB design.
Hi Riccardo,
Most likely all those supply pins are required to be connected on the LTC6400. However, I've reached out to folks who have more history with this part and if I hear otherwise, I'll post here in the next day or so.
Regards,
Hooman
All the V+ and V- pins must have a PCB trace to minimize trace resistance and inductance.
All the V+ and V- pins must have a PCB trace to minimize trace resistance and inductance.