Hi.
Can I use ADA4528 as current monitor circuit or is there a better choice?
Here's a deal.
I wanted to use the ADA4522 (Figure 84 in datasheet), but it has a minimum power supply threshold of 4.5 V. My ADC can handle a maximum of 3 volts.
So I find quite similar OpAmp with 2.5-5.5V power supply voltage - ADA4528.
Сan 4528 be used in the same scheme as 4522?
(Parameters: Rs=10 mOhm, max load less than 5 Amps, R1,R3=1k, R2,R4=50k, so Gain is 50, up to 2.5V to ADC)