Hi all,
Is it acceptable to connect the -Vs supply input of the AD9631 to ground (and let's say +Vs = +3.3V)? I would like to remove a -3.3V supply from my board which has an AD9631 on it and just use ground as -Vs. Currently, I have a 200 ohm resistor from output (pin 6) to negative input (pin 2) and the input signal on positive input (pin 3). The input signal will now be positive going 0-2V range.
Will I run into problems doing this?
Thanks!