AD8138 evaluation board question

Hi,

I am trying to use AD8138 to drive a ADC. I bought the evaluation board for it. I have a little problem regarding the board schematic in the user guide.

On the board, there is a SMA connector which is connected to the pin 7 of the DUT AD8138. There are also some resistors connected with it. But pin 7 of AD8138 is no-connection in the datasheet. I also checked the other datasheet of AD8131, AD8132, AD8139. The pin 7 of these devices are also no-connection. So my question is what this SMA connector is used for?

Thanks,

Sindy