Post Go back to editing

Driving analog data convertor AD7823 with an op-amp

Hello,

I'm interested in using an op-amp to drive an AD7823 data convertor.

Maximum gain required is about ~30, since I can use a ref voltage as low as 1.2V on the AD7823. Required bandwidth operation is 100KHz.

I have no requirements on the op-amp except that the supply range should be between 3v to 5v. However, I do prefer to use a single supply op-amp. I'm not sure whether I should choose an op-amp with a differential output, which according to my understanding, will be more accurate (Will the AD7823 be able to work with it?) or a single ended output with a common ground to the ADC Vin- input?

After reading some application notes I became a little bit confused with all the configurations out there and would appreciate some help...

Thanks in advance,

regards,

Eyal

Parents
  • I would look at the AD8031, MAX4124 or MAX4125, LT6233, MAX4488, ADA4851 or the LT6202. They will all comfortable provide x20 amplification at 100kHz with at least a factor of 10 excess loop gain.

    Instead of making all your signals 0V referenced you could generate a virtual ground reference somewhere between 0.1V and 0.5V above 0V and then configure the front end amp as a differential amplifer rather than a simple non-inverting amplifier. This would raise the opamp output up but a small amount, bypassing the problem of not swinging right down to ground. The ADC negative input would obviously connect to the virtual ground.

    Using a differential amplifier arrangement also provides an easy way of removing ground noise between different parts of your system.

Reply
  • I would look at the AD8031, MAX4124 or MAX4125, LT6233, MAX4488, ADA4851 or the LT6202. They will all comfortable provide x20 amplification at 100kHz with at least a factor of 10 excess loop gain.

    Instead of making all your signals 0V referenced you could generate a virtual ground reference somewhere between 0.1V and 0.5V above 0V and then configure the front end amp as a differential amplifer rather than a simple non-inverting amplifier. This would raise the opamp output up but a small amount, bypassing the problem of not swinging right down to ground. The ADC negative input would obviously connect to the virtual ground.

    Using a differential amplifier arrangement also provides an easy way of removing ground noise between different parts of your system.

Children
No Data