ada4927-1 adding dc offset onto inverting input to maximize adc range

Dear Sir/Madam,

With fully differential current feedback amplifiers like the ADA4927-1 are there any potential problems with adding an positive offset to the inverting input? The use case would be a unipolar input 0 to 1V on the non-inverting input and a 0.5V offset added to the inverting input. With a gain of 2 the full ADC range could be used (ADC with 2Vpp differential). If multiple FDAs are used in this configuration would it be better to use:

a) One LDO for all the FDAs offset

b) One LDO for each FDA offset

c) One LDO for all FDAs buffered using a unity gain buffer for each FDA?

If the unity gain buffer is the better solution would this device require any special attention ie. bandwidth

Thanks Grant

Parents Reply Children
No Data