Post Go back to editing

AD822 max. Output Current

Hi,

I'm referring to the official datasheet of the AD822 operational amplifier.

https://www.analog.com/media/en/technical-documentation/data-sheets/AD822.pdf

It states a minimum value of 15 mA of output current, but no typical or maximum value is given and I cannot find another statement about output current.

I'm interpreting this as that the unit is guaranteed to be able to put out at least 15 mA. Am I right here?

My actual question is about the maximum output current: I would like to use the AD822 as a current source for 4..20 mA signals. Is this possible?

Thank you very much for any help!!