Hi,
I have used these component to design a sinusoidal current generator 0-2Arms 50Hz-2kHz.
I need to have a very low offset (DC component), max 300-400uA.
Could you give me help to low the offset?
Best Regards
LTC6090
Recommended for New Designs
The LTC6090/LTC6090-5 are high voltage, precision monolithic operational amplifiers. The LTC6090 is unity gain stable. The LTC6090-5 is stable in noise...
Datasheet
LTC6090 on Analog.com
LT1006
Production
The LT1006 is the first precision single supply operational amplifier. Its design has been optimized for single supply operation with a full set of specifications...
Datasheet
LT1006 on Analog.com
LTC2057
Recommended for New Designs
The LTC2057 is a high voltage, low noise, zero-drift operational amplifier that offers precision DC performance over a wide supply range of 4.75V to 36V...
Datasheet
LTC2057 on Analog.com
Hi,
I have used these component to design a sinusoidal current generator 0-2Arms 50Hz-2kHz.
I need to have a very low offset (DC component), max 300-400uA.
Could you give me help to low the offset?
Best Regards
Hi,
This is a duplicate thread, continue discussing here LTC6090 LT1006 LTC2057.
Regards,
Goz