Followed the design from Figure 68 of the datasheet to simulate the circuit in LTSpice. The design is included.
It should work from 735uA (5mV output) to about 70mA (4.76V output). The input is a sinusoidal wave of 1kHz, and TIA is powered from ±5VDC.
At lower input current, the output holds as expected; however, as the input current increases, the output is severely distorted. Furthermore, the output does not swing past +4V.
What might be causing this issue in this design, and how to correct the mistakes.
I followed the suggestions from the datasheet but cannot get it to work.
Thanks.
Link to LTSpice schematic:
https://drive.google.com/file/d/11_Q2BlXrEec6JrLpHJhos5Hx-T3i8suF/view?usp=sharing