Post Go back to editing

Re: Driving ADC, please help

Hi Ramon,

You could use a basic inverting opamp config with the ADA4841-1

http://www.analog.com/static/imported-files/tutorials/MT-213.pdf

Rin would be twice Rf. You could use 5V and ground as the supplies. However the limitations are you may lose some range near ground and near 5V (maybe 50-100mV depending on head/footroom spec). Also the input impedance is dictated by Rin, so not a high impedance input. Is the positive supply fixed at 12V?

Best Rgds,

Alan

Parents
  • Hi Alan.

    ADA4841-1 at 5V supply has only an input voltage range of -0.1V to 4V. So, I am not sure what would be the available signal range of 10V input signal after level shifting to 3.33V.

    I am looking now at AD8275 (level translator) and AD8475 (funnel amp). AD8275 has 0.2x gain (1/5), and AD8475 has two gain (attenuation) options of 0.8x and 0.4x. But datasheet only talks about bipolar inputs and differential outputs. I want just only to convert a unipolar input and get single ended output.

    Maybe I could just use a 1/4 precision resistor divider network and buffer? What do you think?

Reply
  • Hi Alan.

    ADA4841-1 at 5V supply has only an input voltage range of -0.1V to 4V. So, I am not sure what would be the available signal range of 10V input signal after level shifting to 3.33V.

    I am looking now at AD8275 (level translator) and AD8475 (funnel amp). AD8275 has 0.2x gain (1/5), and AD8475 has two gain (attenuation) options of 0.8x and 0.4x. But datasheet only talks about bipolar inputs and differential outputs. I want just only to convert a unipolar input and get single ended output.

    Maybe I could just use a 1/4 precision resistor divider network and buffer? What do you think?

Children
No Data