Article In datasheet, it shows MAX2679 is for 1.575G only. Can I use it for 1.2G~1.6G? Or it is narrow band only?



There is no NF vs Frequency curve in datasheet. MAX2679 is optimized on 1575MHz only. It is difficult to compatible design for two band (1258~1563MHz), it may influence the performance. 
According to the curves below, the gain error is around 3~4dB at 1258~1563MHz.


  1. S22 参数优化在1575MHz,


     

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.