Article Mesaure AC Line Current (230V AC)

Question

Is it possible to use the ADuM3190 to measure current in 230V AC line?

Answer

The ADuM3190 was designed for a 0.35V to 1.5V input, while the 230VAC current
from a resistor would have a positive and negative voltage, and would probably
be a low voltage to keep losses in the resistor low. Even if the voltage
measured was unipolar, the errors of gain at more than 15%, plus offset and
linearity errors from the ADUM3190 when not used as designed as an isolated
feedback amplifier, may be too large for the application.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.