Article Why is the ADuM3190/4190 supply voltage range different than the operating voltage range?

Question

Why is the ADuM3190/4190 supply voltage range different than the operating
voltage range?

Answer

The supply voltage range is a wide 3V to 20V through the use of an internal
voltage regulator that inputs voltages up to 20V and has a 3V regulated
output. There are 3V regulators on each side of the ADuM3190/4190 which supply
the precision circuits of the isolated error amplifier.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.