Article controlling the WB pin on the AD8237

Question

Part Number: AD8237


Can the BW pin of AD8237 be controlled with a GPIO on a MCU?




Answer

We see no problem with this. Advisable to use a pull-up resistor of about
4.7k ohms to the BW pin and interface to a microprocessor to control this
pin. e.g. control and output high or low to simulate this Vs or -Vs (gnd)


The BW pin is one input of a comparator. It is high-Z, there are no current
driving requirements, and there are no minimum rise/fall time requirements. The
other input of the comparator is at a resistor divider from +Vs to –Vs, which
creates a half-supply voltage for comparison.

Threshold voltages: High is (+VS + (–VS))/2 + 60mV min, Low is (+VS + (–VS))/2
– 60mV max (this takes into account worst-case process variation and also 30mV
of hysteresis)

Propagation delay: typically 10µs comparator propagation delay + the settling
time of AD8237 in the final configuration

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.