Article AD8221 output impedance

Question

Could you please provide me data on the resistance of the output path of the
AD8221?

Answer

The output resistance is quite low at dc and low frequencies. Approximately 0.1
ohms until the short circuit current limit kicks in above about 18mA. As the
frequency increases, the output resistance increases too as the open-loop gain
decreases. It’s about 150 ohms at 1MHz and it can be traced back 20dB/decade
from there, meaning 15 ohms at 100kHz, 1.5 ohms at 10kHz, and so on.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.