Article AD8221: Driving capacitive loads

Question

Can you say advise about stability of the AD8221 at capacitive loads. Which
capacitive load is acceptable?

Answer

The settling time plots in the datasheet are all done with a 100pF load, and
the part is very stable with this much capacitance or less. According to our
Engineers AD8221 could probably drive about a nanofarad before going unstable
(note this has not been tested in lab).

To drive a larger capacitive load, one small resistor is recommended between
the AD8221 and the capacitor. Best way to determine the correct resistor value
is empirically using a square wave input into the AD8221 and adjusting the
resistance until the square wave looks reasonable at the output.

(There is a note on driving a cable on page 21 of AD8222 datasheet (dual of
AD8221),you may also find this useful).

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.