Article AD822: Output voltage exceeds rails

Question

In an amplification circuit with AD822 supplied with +15V/-15V, there could be
an operating condition in which the output of the op-amp is saturated to +15V
(Vin is so high that Vin*G>15V). Besides, in this situation, the output could
be connected through a pull-up resistor of about ten kilohms to a voltage
source higher than +15V. How does the op-amp behave in this conditions and what
is the limit of the value of the voltage applied through the 10kOhm resistor to
the output of the op-amp so not to damage the op-amp?

Answer

The output of an op-amp should not go outside its supply rails as it may
destroy the device. If the load resistance is such that the pull-up resistor
current flows in the load and does not cause the terminal to rise above the
op-amp supply then the voltage on the resistor is unimportant. If you wish the
OP to rise above the rail - do not do it!

It would be sensible to use a schottky diode clamp to prevent the output rising
too high by accident.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.