Article AD8131: CM input resistance

I’m trying to find out the CM_input resistance value of AD8131 and AD8138. I’m
driving 10 ad8131 CM inputs with a single 2.5V reference chip. The max current
this reference module can output is 30mA.  I would be grateful if you could let
me know the CM_input resistance value of an AD8131 and of AD8138.

 

This parameter is actually specified, but I agree that it is somewhat difficult
to find out where it is in the data sheet.
On pages 2 and 3 of each data sheet are the specs: +/-5V supplies on page 2 and
+5V supply on page 3.
There are two bold headings in the Parameter column. At the top is +/-Din...
and 2/3 of the way down is Vocm to +/-OUT Specs. These mean that the top
section is for the differential input operation and the bottom is for the Vocm
operation. I don’t think that this is so clear in the way these specs are dealt
with.
Under the Vocm specs is a Parameter “Input Resistance”. I believe that this is
what you want.
In case you’re wondering why there is a difference in this between 10V supplies
and 5V supplies: Vocm is biased at mid-supply by FET devices operating in their
pinch-off region. These change resistance vs. bias voltage.
Also, the AD8138 impedance is higher, but it has a higher offset voltage when
Vocm floats. This is not specified on pages 2 and 3 as for the AD8131, but it
is addressed on page 10 in the paragraph: “Setting the Output Common-Mode
Voltage”.
If it is desired to have a more accurate Vout,cm, then Vocm should be directly
biased and do not rely on the internal bias.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.