Article REF195: PIN layout

Q 

How the first pin on SOIC8 is marked? I try to use REF195GS and can't find
first pin because it is not marked by a point

 

A 

You will see that one of the edges of the plastic package is cut at 45 degrees
above the pins (bevelled or tapered) while the other edge is cut at 90 deg as
normal.

The edge which is cut at 45deg indicates the pin 1 location. You can see this
on page 23. The diagram on the right, which shows the SOIC package from the
end, shows that the left hand edge is tapered while the right hand edge is
nearly at 90deg.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.