MAX9939AUB+T: FAQ

  • Can we detect +/-0.2mV using MAX9939

    You can input MAX9939 with +/- 0.2mV (INA+ and INA-) but ensure the gain is set to higher value and the corresponding offset values are set as mentioned in data sheet page 9 and 10
  • What is the GBW of the MAX9939?

    The typical GBW depends on the programmed gain value. For gain values of 0.2V/V and 1V/V, the GBW is 2.15MHz. For gains of 157V/V, the GBW is 279MHz. Curves with this information can be found on page 4…

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.