Article Can I use a strain gauge with the MAX1452?

Any type of sensor can be used, as long as the sensor excitation and sensor output comply with the signal conditioner's requirement. These signal conditioners operate on the differential input between the INP and INM pins. For example, the MAX1452 has been utilized in applications using 350Ω strain gauge.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.